MPC8313 GPCM LCLK Output Jitter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8313 GPCM LCLK Output Jitter

2,090 Views
wonderwizard
Contributor III

Is there any information on how much jitter can be expected on the GPCM LCLK output.

I couldn't find any information in the MPC8313EEC (MPC8313E PowerQUICC II Pro Processor Hardware Specifications, Rev. 4)

Thanks

Chris

Labels (1)
Tags (4)
0 Kudos
Reply
4 Replies

1,809 Views
LPP
NXP Employee
NXP Employee

We do not have the 83137 LCLK jitter specs

However some measurements have been done:

Average jitter is 230ps, max jitter 420ps

0 Kudos
Reply

1,809 Views
wonderwizard
Contributor III

Are those jitter measurements made from the MPC8313E reference design board? And are they RMS or Pk-Pk?

0 Kudos
Reply

1,809 Views
wonderwizard
Contributor III

Bump, RMS or PK-PK?

0 Kudos
Reply

1,809 Views
LPP
NXP Employee
NXP Employee

Maximum was Pk-Pk value.

0 Kudos
Reply