MPC8313 GPCM LCLK Output Jitter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8313 GPCM LCLK Output Jitter

2,928件の閲覧回数
wonderwizard
Contributor III

Is there any information on how much jitter can be expected on the GPCM LCLK output.

I couldn't find any information in the MPC8313EEC (MPC8313E PowerQUICC II Pro Processor Hardware Specifications, Rev. 4)

Thanks

Chris

ラベル(1)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

2,647件の閲覧回数
LPP
NXP Employee
NXP Employee

We do not have the 83137 LCLK jitter specs

However some measurements have been done:

Average jitter is 230ps, max jitter 420ps

0 件の賞賛
返信

2,647件の閲覧回数
wonderwizard
Contributor III

Are those jitter measurements made from the MPC8313E reference design board? And are they RMS or Pk-Pk?

0 件の賞賛
返信

2,647件の閲覧回数
wonderwizard
Contributor III

Bump, RMS or PK-PK?

0 件の賞賛
返信

2,647件の閲覧回数
LPP
NXP Employee
NXP Employee

Maximum was Pk-Pk value.

0 件の賞賛
返信