MPC8309 SD/MMC/SPI Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 SD/MMC/SPI Boot

2,119 Views
ganjiaravind
Contributor I

Hi everyone ,when MPC8309twr Board need to Boot from SD/MMC or SPI device there should be a configuration dat file,among all configuration offsets i have a question over the offsets 0x50,0x58,0x60.

offset 0x50 ---- Source address

offset 0x58 ---- Target address

offset 0x60 ---- Execution starting address

what exact values to be used in this offsets or is there any procedure to calculate ,

thank you in advance.

0 Kudos
Reply
1 Reply

1,938 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Please check Booting with sd card in MPC8309twr It provides example of the dat file.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply