MPC8309-KIT development board, eLBC the mpc8309 enhanced local bus controller bus four chip select signal: MPC SOM MPC_SOM_LCS2#, MPC LBC MPC_LBC_CS3#, MPC LBC MPC_LBC_CS4#, MPC LBC MPC_LBC_CS5# corresponding base address.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309-KIT development board, eLBC the mpc8309 enhanced local bus controller bus four chip select signal: MPC SOM MPC_SOM_LCS2#, MPC LBC MPC_LBC_CS3#, MPC LBC MPC_LBC_CS4#, MPC LBC MPC_LBC_CS5# corresponding base address.

Jump to solution
1,273 Views
dongpolu
Contributor I

MPC8309-KIT development board, eLBC the mpc8309 enhanced local bus controller bus four chip select signal: MPC SOM MPC_SOM_LCS2#, MPC LBC MPC_LBC_CS3#, MPC LBC MPC_LBC_CS4#, MPC LBC MPC_LBC_CS5# corresponding base address.

0 Kudos
Reply
1 Solution
1,109 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes the MPC8309 eLBC has four chip select signals. The MPC830x-KIT may support greater than 4 because it may support several MPC830x device. So MPC8309-KIT has MPC_LBC_CS0# --- MPC_LBC_CS3#. See excerpt from the schematics.

MPC8309_4_LCS.gif On start up only when the MPC8309 boot from the local bus only bank0 has predefined boot settings which you can see in the MPC8309 reference manual. Other eLBC banks are not enabled by default. Software has to set local bus banks base addresses and sizes. You should look for these settings the board documentation and software documentation you run on the board. See attached excerpt from the MPC8309-kit user guide

MPC8309Kit_memmap.gif

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,109 Views
dongpolu
Contributor I

Thanks to Podiatchev Serguei!

0 Kudos
Reply
1,110 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes the MPC8309 eLBC has four chip select signals. The MPC830x-KIT may support greater than 4 because it may support several MPC830x device. So MPC8309-KIT has MPC_LBC_CS0# --- MPC_LBC_CS3#. See excerpt from the schematics.

MPC8309_4_LCS.gif On start up only when the MPC8309 boot from the local bus only bank0 has predefined boot settings which you can see in the MPC8309 reference manual. Other eLBC banks are not enabled by default. Software has to set local bus banks base addresses and sizes. You should look for these settings the board documentation and software documentation you run on the board. See attached excerpt from the MPC8309-kit user guide

MPC8309Kit_memmap.gif

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply