MPC8308NSG Zigbee communication & PHP services adding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8308NSG Zigbee communication & PHP services adding

1,324 Views
ziedjelassi
Contributor II

Hi All,

I have an MPC8308NSG Box. I have to check its Zigbee connectivity and integration some php pages.

To begin, I have generate a new uImage using the given DVD. When I add php package, the Box will be pumped in the following message:

Instruction dump:

38800007 38630118 4bfaa0ed 80010014 38210010 7c0803a6 4e800020 81630118

71600088 68000088 7c0000d0 54000ffe <0f000000> 3920ff77 7d6b4838 91630118

VFS: Cannot open root device "mtdblock2" or unknown-block(31,2)

Please append a correct "root=" boot option; here are the available partitions:

1f00            1024 mtdblock0 (driver?)

1f01            7168 mtdblock1 (driver?)

1f02           32768 mtdblock2 (driver?)

1f03              32 mtdblock3 (driver?)

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(31,2)

Rebooting in 180 seconds..

Actually, I'm using an uImage containing the default configuration added to apach and mysql packages.

then, I'm trying to check zigbee internal module.

the MPC8308NSG zigbee LED is blinking and using a zigbee sniffer I can not detect it.

Best regards,

Zied.

0 Kudos
Reply
0 Replies