MPC8308 with LCD controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8308 with LCD controller

1,998 Views
fernandoalcaide
Contributor II

Dear, I want to use MPC8308 power QICC and I want to conect to LCD. does  power Quicc have "LCD controller"? Can you sent me information about this module?. I do not find information for this.

1 Reply

1,930 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The MPC8308 does not have LCD controller. There is separate LCD module

http://cache.freescale.com/products/power-architecture-processors/powerquicc-processors/powerquicc-i...

which was designed for the TWR-MPC8309(MPC8306) Industrial Networking Development Platform.

There are P1022 and P1013 which have internal LCD controller. See also LS1021A.

For quick review of available powerQUICC devices see the Processor Selector Guide

http://cache.freescale.com/files/32bit/doc/brochure/PWRARCHQIQSG.pdf

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------