MPC8308 's hardware question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308 's hardware question

1,135件の閲覧回数
bsw_0204107
Contributor I

hi! in MPC8308, can I dirrectly use one USB without PHY?

タグ(1)
0 件の賞賛
返信
1 返信

1,084件の閲覧回数
Pavel
NXP Employee
NXP Employee

The MPC8308 USB ULPI cannot be connected to other USB ULPI controller. The MPC8308 USB ULPI control signals are inputs: USBDR_PWR_FAULT, USBDR_CLK, USBDR_DIR and USBDR_NXT. See the Table 13-1 of the MPC8308 Reference Manual.

It required using a USB ULPI PHY.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信