MPC8308 programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8308 programmer

1,820 Views
venkateshn
Contributor II

Hi,

kindly let me know the compatibility of  CWH-UTP-PPCD-HE USB TAP to MPC8308CVMAFDA processor with CWH-CTP-COP-YE probe tip.

0 Kudos
Reply
2 Replies

1,669 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello VENKI N,

It seems that I didn't provide the exact information previously.

CodeWarrior TAP is the replacement of previous products USB TAP, USB TAP for MPC83xx is not manufactured any more.

Currently USB TAP(CWH-UTP-PPCD-HE) is only used for DPI Power Architecture(MPC8xx).

For MPC8308 you need to purchase CodeWarrior TAP(CWH-CTP-BASE-HE) with probe CWH-CTP-COP-YE.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,669 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello VENKI N,

CodeWarrior TAP is compatible with MPC8308, and you need to use CodeWarrior 8.8 for this processor.

If the user wants to use CodeWarrior TAP in CodeWarrior 8.8, Patch 8.8.6 needs to downloaded and installed, please download the Patch from

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-POWER-NETWORKING&fpsp=1&tab=Design..., and click Product Download-> Select Windows professional edition->click Agreement to get Patch 8.8.6.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply