MPC8308 Support for Non-OS based applications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308 Support for Non-OS based applications

ソリューションへジャンプ
2,807件の閲覧回数
venkateshn
Contributor II

Hi,

I am planning to use MPC8308 processor for Non OS (Firmware) based standalone applications, kindly let me know the suitability of this part.

Regards,

Venkatesh N

ラベル(3)
0 件の賞賛
返信
1 解決策
2,529件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, MPC8308 is suitable for standalone applications.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
2,529件の閲覧回数
venkateshn
Contributor II

Dear alexander.yakovlev,

can you suggest me the standalone application IDE and Compiler for MPC8308 processor.

Note: please share me the standalone example codes.

Regards,

Venkatesh N

0 件の賞賛
返信
2,529件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

We recommend using our CodeWarrior software for that purpose:

CodeWarrior Development Tools for PowerQUICC|Freescale

Please look default "Hello World" project in CodeWarrior for standalone project example code.

2,529件の閲覧回数
venkateshn
Contributor II

Hi,

I have installed CodeWarrior 8.8.5version. But i did not find any Hello World example for MPC8308 in installed CW folder.

Please share me the link or NON OS based examples to realize all interfaces related to Evaluation board (MPC8308RDB).

Thanks & Regards,

Venkatesh N

0 件の賞賛
返信
2,529件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please press "File" - "New", enter project name and location, and select "EPPC New Ptoject Wizard". On the next screen select Freescale linker, than on the next screen - MPC83xx tab, MPC8308 device and board you are using, than language type C or C++ and debug probe type. Finally, generated default project will be standalone application for bare board.

0 件の賞賛
返信
2,529件の閲覧回数
venkateshn
Contributor II

alexander.yakovlev

alexander.yakovlev i have purchased MPC8308-RDB Evaluation board for my application development but it is of OS based so can you share any MPC8308 Non OS based applications for my reference.

Regards,

Venkatesh N

0 件の賞賛
返信
2,530件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, MPC8308 is suitable for standalone applications.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------