MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?

1,972 次查看
jmaccedian
Contributor I

We're using the MPC8308. There is a confusion between the datasheet and some schematic about the supply for the eTSEC1 in RGMII mode. Can we connect the eTSEC1 at 3.3V in RGMII mode? or it's only 2.5V? LVDD1 = NVDDC = TSEC1 = ? in RGMII mode


JMAccedian

标签 (1)
标记 (5)
0 项奖励
回复
1 回复

1,355 次查看
andrei_skok
NXP Employee
NXP Employee

According to the MPC8308 Datasheet:

"The RGMII interface is defined for 2.5 V, while the MII interface can be operated at 3.3 V"

If you use eTSEC1 in RGMII mode you should connect LVDD1 (NVDDC) to 2,5V.

0 项奖励
回复