MPC8306 UCC problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8306 UCC problem

3,162件の閲覧回数
gangadhar1
Contributor I

we programmed both the ucc in hdlc mode(NMSI) . when both ucc are enabled simultaneously, one of the ucc stops working.please let us know any fix is necessary.  Development environment used is LTIB software.

I am getting CRC ERROR on UCC5(enabled first) and UCC7 is working fine.

hdlc0 Link encap:Point-to-Point Protocol
inet addr:10.0.0.1 P-t-P:10.0.0.2 Mask:255.255.255.0
UP POINTOPOINT NOARP MTU:1500 Metric:1
RX packets:0 errors:0 dropped:14 overruns:0 frame:14
TX packets:30 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:16

RX bytes:0 (0.0 b) TX bytes:88 (88.0 b)

hdlc1 Link encap:Point-to-Point Protocol
inet addr:20.0.0.1 P-t-P:20.0.0.2 Mask:255.255.255.0
UP POINTOPOINT RUNNING NOARP MTU:1500 Metric:1
RX packets:292 errors:0 dropped:0 overruns:0 frame:0
TX packets:293 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:16

RX bytes:3504 (3.4 Kb) TX bytes:3504 (3.4 Kb)

Packets are dropped due to CRC error in BD's.

please suggest how to fix this.

0 件の賞賛
返信
3 返答(返信)

2,885件の閲覧回数
Sw2
Contributor I

Hi @gangadhar1 ,

We are faced the similar issue.

How did you fix this problem?

Thanks

0 件の賞賛
返信

3,036件の閲覧回数
gangadhar1
Contributor I

We did try 64KHz(minimum frequency we can try )clock  rate but results are same CRC errors on RX side.
For your reference I am attaching schematics

Gangadhar

0 件の賞賛
返信

3,036件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. Please submit me your UCC external connections schematic for analysis.

2. Please try reducing transmission speed (transmission frequency) at remote side (at the side, which is used for transmission the data, which is received with errors). Please try reducing this frequency for short time, for test purposes only. I do understand that your design can not be used at this reduced frequency, however please test this to distinguish between error caused by QE overload and error caused by configuration errors. Please check if the problem appears at reduced frequency to exclude overload-related erratic behavior.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信