MPC8270 Clock of processor core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8270 Clock of processor core

Jump to solution
3,442 Views
Amit-Kumar
Contributor II

Hi,

We are trying to know from the software the clock the processor core is running at for this processor:

Processor Version Register (PVR) = 0x80822014 (mpc8270/8280)

I looked at the reference manual but doesn't seem like we have a quick register to read that. From code there appears to be a hardcoded value which is used with multipliers to get the other clock values. Please confirm if there is any register for this ?

I think it is referred as "CLKIN" external input in manuals.

Labels (1)
0 Kudos
Reply
1 Solution
3,435 Views
ufedor
NXP Employee
NXP Employee

> We are trying to know from the software the clock the processor core is running at for this processor

Sorry, the request is not clear.

CLKIN frequency can't be determined by software means.

Core multiplication factor could be read from the SCMR[CORECNF].

View solution in original post

2 Replies
3,391 Views
Amit-Kumar
Contributor II

Thanks.

0 Kudos
Reply
3,436 Views
ufedor
NXP Employee
NXP Employee

> We are trying to know from the software the clock the processor core is running at for this processor

Sorry, the request is not clear.

CLKIN frequency can't be determined by software means.

Core multiplication factor could be read from the SCMR[CORECNF].