MPC8260 processor and a 256Mbyte SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8260 processor and a 256Mbyte SDRAM

2,601件の閲覧回数
murattemiz
Contributor I

 In an application a costumer will use an MPC8260 processor and a 256Mbyte SDRAM (4 x MT48LC32M16A2 parallel) via the existing SDRAM interface. The SDRAM will operate at a frequency of 50MHz. (The SDRAM is already controlled in another application with another processor and should be used in this case again if possible.) The "self-refresh" function is important. From the data sheets I could see that the interface of the processor does not provide a CKE pin, which is used by the SDRAM.  So the question whether the specified SDRAM is compatible with the MPC8260 SDRAM interface and how the corresponding application would be implemented? Or is there an alternative SDRAM that is more suitable for this purpose?  Many thanks in advance.

ラベル(1)
  • DDR

0 件の賞賛
返信
5 返答(返信)

2,381件の閲覧回数
murattemiz
Contributor I

According to the datasheet of the SDRAM, however, the CKE pin would have to be actively controlled, which is why I suspect that a 1KOhm resistor should not be sufficient for VDD?

MT48LC32M16A2.jpg

Enclosed are the sections from the data sheet of the SDRAM (MT48LC32M16A2).

 

0 件の賞賛
返信

2,381件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no way to implement Self Refresh mode for SDRAM without external glue logic. The problem is that Self Refresh command couldn't be implemented without synchronous (with SDRAM clock) control of the Clock Enable SDRAM input (CKE).

Below is possible variant of the "glue logic" which allows to put SDRAM into Self Refresh mode. During normal operation Output port pin level is high. When Self Refresh is required, Output port pin level is set to low. In this case CKE will be lowered synchronously with SDRAMCS.

CKE.gif

0 件の賞賛
返信

2,381件の閲覧回数
murattemiz
Contributor I

Do you have any experience with this logic acc. self refresh mode in SDRAM? If yes, could you give me please the Info which SDRAM did you use. 

And are you sure, that this logic will work in this case? I am not sure if the timing can handle this mode.....

0 件の賞賛
返信

2,381件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Do you have any experience with this logic acc. self refresh mode in SDRAM?

Unfortunately, no.

0 件の賞賛
返信

2,381件の閲覧回数
ufedor
NXP Employee
NXP Employee

The MT48LC32M16A2 can be used.

The CKE pin can be connected to VDD through 1 kOhm resistor.

0 件の賞賛
返信