MCP7448 60x amount of bytes to tranfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCP7448 60x amount of bytes to tranfer

866件の閲覧回数
addi
Contributor I

Im going to simulate MCU working under 60x bus.

But according to the documentation I can't get understanding in the following data transfer modes:

1) burst dara transfer, - up to 32 bytes or 32 bytes only?

2) single beat, - from 1 byte and up to 8 bytes?

3) double beat, -  up to 16 bytes or 16 bytes only?

4) L2 cache reading/writing  is only possible in burst mode? 

 

Please help in  understanding

0 件の賞賛
返信
2 返答(返信)

710件の閲覧回数
addi
Contributor I

Thank you fro your replay!

I checked this document in relating of my question and unfortunally didn't find the answer still

Thus I asking to correct me in the following assignments of my understanding:

1) burst dara transfer is for L2 cache reading/writing

2) single beat is in range from 1 byte and up to 8 bytes

3) L2 cache reading/writing is only possible in burst mode

4) L2 cache reading/writing is possible in four or more bus cycles

 

0 件の賞賛
返信

821件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信