Kernel Update in MPC8323E-RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Update in MPC8323E-RDB

1,526件の閲覧回数
narreddisivapra
Contributor II

Hi,

      Can any one help me in updating 2.6.20-kernel to higher version for the development board MPC8323E-RDB.? I am using MPC8323E-RDB board and I downloaded ISO image from nxp website. I built this with LTIB and finally I got the linux kernel with 2.6.20 version. In the progress of driver development of I am facing some issues with this versions for example that it not supporting some Kernel-APIs. I didn't find any other option for selecting other than 2.6.20 kernel while kernel configuration using LTIB.

Please, help in updating the kernel to higher supportive kernel to this development board.

Thanks and Regards,

Siva Prakash Reddy Narreddy

タグ(3)
0 件の賞賛
返信
1 返信

1,427件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at information on the following pages

http://www.berkes.ca/guides/linux_kernel.html

http://www.bitshrine.org/autodocs/LtibFaq.html

https://freescale.jiveon.com/thread/28758

http://ltib.nongnu.narkive.com/8XSfiWTA/how-to-upgrade-the-kernel-to-2-6-21-on-mpc8349e-board

https://lists.gnu.org/archive/html/ltib/2011-11/msg00019.html

https://lists.gnu.org/archive/html/ltib/2007-07/msg00009.html

https://lists.nongnu.org/archive/html/ltib/2008-11/msg00013.html

 

See also the following:

http://ltib.org/pages/LTIB_generic_v1.4_-_version_6.4.1.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN3765.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信