¿It is possible to reinitialize the DDR controller on the MPC8548 just after his initialization? ¿How could i do that?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

¿It is possible to reinitialize the DDR controller on the MPC8548 just after his initialization? ¿How could i do that?

1,176 次查看
diegomartin
Contributor I

This is what a want to do:

1) Initialize DDR controller with no ECC and no init memory..

lis r7, 0x43000008@ha
ori r7, r7, 0x43000008@l
stw r7, DDR_SDRAM_CFG(r6)

lis r7, 0x04400000@ha
ori r7, r7, 0x04400000@l
stw r7, DDR_SDRAM_CFG_2(r6)

lis r7, 0xC3000008@ha
ori r7, r7, 0xC3000008@l
stw r7, DDR_SDRAM_CFG(r6)

2) Just After the initializacion, i want to check ram and reinitialize de DDR controler witch ECC and memory initialization. I'm trying this for the reinitialization:

lis r7, 0xC300000A@ha
ori r7, r7, 0xC300000A@l
stw r7, DDR_SDRAM_CFG(r6)

lis r7, 0x4300000A@ha
ori r7, r7, 0x4300000A@l
stw r7, DDR_SDRAM_CFG(r6)

lis r7, 0x6300000A@ha
ori r7, r7, 0x6300000A@l
stw r7, DDR_SDRAM_CFG(r6)

lis r7, 0x04400010@ha
ori r7, r7, 0x04400010@l
stw r7, DDR_SDRAM_CFG_2(r6)

lis r7, 0xE300000A@ha
ori r7, r7, 0xE300000A@l
stw r7, DDR_SDRAM_CFG(r6)

lis r7, 0xE3000008@ha
ori r7, r7, 0xE3000008@l
stw r7, DDR_SDRAM_CFG(r6)

Sometimes it works fine and other times it hangs saying that the memory is nos available.

Thank you in advance.

标签 (1)
0 项奖励
回复
1 回复

1,025 次查看
r8070z
NXP Employee
NXP Employee

DDR3_init_flow.jpg

From the DDR3 initialization flow we see that MEM_EN bit starts DDR3 device full initialization which supposed that  DDR3 device has been reset. I think your experiment confirms that. Re-initialization should starts from the DDR3 Reset.

0 项奖励
回复