Issues in SPI Boot on custom T2081

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues in SPI Boot on custom T2081

1,752 次查看
Irfan3
Contributor III

Hi Team,

We are working on SPI NOR boot in T2081 custom board.
 
We were able to load the U-boot into the SPI NOR device and it was running till DDR Initialization failed.
 
While DDR debug due to DDR init fail, with some changes in hardware, now we are not able to boot-up at all.
 
We have cross checked the dump of the flashed file with the input file and it's same. Also, we have checked the loaded file and configuration of PBL from software side, it's not changed at all.
 
Could you please suggest us how to debug this issue.
 
Thanks and Regards,
Irfan
0 项奖励
回复
1 回复

1,742 次查看
ufedor
NXP Employee
NXP Employee

> While DDR debug due to DDR init fail, with some changes in hardware

Which exactly hardware changes?

0 项奖励
回复