Issue with Hotplug Package in LTIB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with Hotplug Package in LTIB

2,772 次查看
narreddisivapra
Contributor II

Hello,

         I am using LTIB for Kernel image building for the bsp "MPC8323E-RDB" and I am using ubuntu 8.10 loaded PC. I built LTIB successfully. Now, I selected the package "udev" in LTIB configure menu and it automatically selected "hotplug" package too. Here, I am facing issue with building "hotplug" package and the kenel log is as follows..

Processing: hotplug
=====================
rpmbuild --dbpath /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rootfs//var/lib/rpm --target ppc --define '_unpackaged_files_terminate_build 0' --define '_target_cpu ppc' --define '__strip strip' --define '_topdir /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm' --define '_prefix /usr' --define '_tmppath /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bb --clean --rmsource /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/dist/lfs-5.1/hotplug/hotplug.spec
Building target platforms: ppc
Building for target ppc
Executing(%prep): /bin/sh -e /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/rpm-tmp.41971
+ umask 022
+ cd /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm/BUILD
+ cd /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm/BUILD
+ rm -rf hotplug-2004_03_29
+ /bin/gzip -dc /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm/SOURCES/hotplug-2004_03_29.tar.gz
+ tar -xvvf -
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/debian/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/hotplug/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/hotplug/pci/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/hotplug/usb/
-rw-r--r-- greg/greg 5194 2004-03-30 00:55 hotplug-2004_03_29/etc/hotplug/hotplug.functions
-rw-r--r-- greg/greg 702 2004-03-12 05:02 hotplug-2004_03_29/etc/hotplug/blacklist
-rwxr-xr-x greg/greg 1129 2004-03-27 04:04 hotplug-2004_03_29/etc/hotplug/firmware.agent
-rwxr-xr-x greg/greg 2873 2004-03-27 04:04 hotplug-2004_03_29/etc/hotplug/ieee1394.agent
-rwxr-xr-x greg/greg 2188 2004-03-30 03:53 hotplug-2004_03_29/etc/hotplug/net.agent
-rwxr-xr-x greg/greg 3746 2004-03-27 04:06 hotplug-2004_03_29/etc/hotplug/pci.agent
-rwxr-xr-x greg/greg 2254 2004-03-27 04:04 hotplug-2004_03_29/etc/hotplug/pci.rc
-rwxr-xr-x greg/greg 1455 2004-03-27 04:38 hotplug-2004_03_29/etc/hotplug/scsi.agent
-rwxr-xr-x greg/greg 13249 2004-03-27 04:06 hotplug-2004_03_29/etc/hotplug/usb.agent
-rw-rw-r-- greg/greg 39129 2004-03-27 04:26 hotplug-2004_03_29/etc/hotplug/usb.distmap
-rw-r--r-- greg/greg 4364 2003-10-08 01:21 hotplug-2004_03_29/etc/hotplug/usb.handmap
-rwxr-xr-x greg/greg 12887 2004-03-30 01:04 hotplug-2004_03_29/etc/hotplug/usb.rc
-rwxr-xr-x greg/greg 3227 2004-03-27 04:04 hotplug-2004_03_29/etc/hotplug/input.rc
-rw-rw-r-- greg/greg 189 2001-01-17 00:52 hotplug-2004_03_29/etc/hotplug/usb.usermap
-rwxr-xr-x greg/greg 6369 2002-08-08 15:35 hotplug-2004_03_29/etc/hotplug/dasd.agent
-rwxr-xr-x greg/greg 685 2002-08-08 15:23 hotplug-2004_03_29/etc/hotplug/dasd.permissions
-rwxr-xr-x greg/greg 6967 2002-10-10 19:13 hotplug-2004_03_29/etc/hotplug/tape.agent
-rwxr-xr-x greg/greg 491 2002-10-08 16:39 hotplug-2004_03_29/etc/hotplug/tape.permissions
-rwxr-xr-x greg/greg 6546 2004-03-27 04:16 hotplug-2004_03_29/etc/hotplug/input.agent
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/hotplug.d/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/hotplug.d/default/
-rwxr-xr-x greg/greg 2924 2004-03-27 04:04 hotplug-2004_03_29/etc/hotplug.d/default/default.hotplug
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/rc.d/
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/etc/rc.d/init.d/
-rwxr-xr-x greg/greg 1160 2003-03-28 05:55 hotplug-2004_03_29/etc/rc.d/init.d/hotplug
drwxrwxr-x greg/greg 0 2004-03-30 04:29 hotplug-2004_03_29/sbin/
-rwxr-xr-x greg/greg 1160 2003-09-25 01:57 hotplug-2004_03_29/sbin/hotplug
-rwxrwxr-x greg/greg 736 2001-06-12 05:30 hotplug-2004_03_29/mkinstalldirs
-rw-r--r-- greg/greg 14351 2004-03-30 04:28 hotplug-2004_03_29/ChangeLog
-rw-r--r-- greg/greg 2591 2003-06-28 05:43 hotplug-2004_03_29/Makefile
-rw-r--r-- greg/greg 8693 2003-03-28 05:55 hotplug-2004_03_29/README
-rw-r--r-- greg/greg 3802 2004-03-12 05:00 hotplug-2004_03_29/hotplug.8
-rw-r--r-- greg/greg 2878 2004-03-30 04:28 hotplug-2004_03_29/hotplug.spec
+ STATUS=0
+ [ 0 -ne 0 ]
+ cd hotplug-2004_03_29
+ exit 0
Executing(%build): /bin/sh -e /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/rpm-tmp.41971
+ umask 022
+ cd /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm/BUILD
+ cd hotplug-2004_03_29
+ make
Built hotplug-2017_05_29.tar.gz
+ exit 0
Executing(%install): /bin/sh -e /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/rpm-tmp.41971
+ umask 022
+ cd /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/rpm/BUILD
+ cd hotplug-2004_03_29
+ rm -rf /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug
+ make install prefix=/home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug//opt/freescale/rootfs/ppc
/usr/bin/install -c -D sbin/hotplug /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug//opt/freescale/rootfs/ppc/sbin/hotplug
/usr/bin/install -c -d /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug//opt/freescale/rootfs/ppc/etc/hotplug/{usb,pci}
/usr/bin/install -c -D etc/hotplug.d/default/default.hotplug /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug//opt/freescale/rootfs/ppc/etc/hotplug.d/default/default.hotplug
for F in etc/hotplug/{*.{agent,rc},hotplug.functions} ; do \
/usr/bin/install -c $F /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/hotplug//opt/freescale/rootfs/ppc/etc/hotplug ; \
done
/usr/bin/install: cannot stat `etc/hotplug/{*.{agent,rc},hotplug.functions}': No such file or directory
make: *** [install] Error 1
error: Bad exit status from /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/rpm-tmp.41971 (%install)


RPM build errors:
Bad exit status from /home/rnd/Desktop/8323/ltib-mpc832x_rdb-20081112/tmp/rpm-tmp.41971 (%install)
Build time for hotplug: 0 seconds

Failed building hotplug


f_buildrpms() returned an error, exiting
traceback:
main:491


Started: Mon May 29 14:30:23 2017
Ended: Mon May 29 14:30:29 2017
Elapsed: 6 seconds

These packages failed to build:
hotplug
Build Failed

Exiting on error or interrupt
rnd@rnd3:~/Desktop/8323/ltib-mpc832x_rdb-20081112$

Please, clear this issue as soon as possible.

Thanks and Regards,

Siva Prakash Reddy Narreddi

标记 (2)
0 项奖励
回复
2 回复数

2,579 次查看
Pavel
NXP Employee
NXP Employee

I have tested NXP LTIB Linux BSP for the MPC823ERDB board: MPC8323E-RDB-20081112.iso

There is no problem for building if "hotplug" is enabled. See attachment.

This LTIB was tested under Ubuntu 10.04.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,579 次查看
narreddisivapra
Contributor II

Sorry, I couldn't find any attachment here. Can you gone through the log what I hand send in first query.? I didn't understood what errors are there in that script.?

0 项奖励
回复