Hi Team,
we are working on the NAND flash device for Custom T2081 board.
The Nand device which we are using is from Micron MT29F8G08ABDA-IFC.
The issue is as follows:
writing at ROW address= 0x10000000 or 0x00001000 IFC_NAND_EVTER_STAT shows NAND operation complete.
whereas while read operation at 0x10000000 IFC_NAND_EVTER_STAT shows NAND operation is not complete.
also while read operation at 0x00001000 IFC_NAND_EVTER_STAT shows NAND operation is complete but with Error as "uncorrectable ECC error due to page read operation".
For reference i am attaching the screenshots of the above mentioned issue.
Please can you suggest me what could be the issue? Also how can we verify at what memory address of nand device it is getting programmed.
Thanks & regards,
Irfan