Is there any code example for TWR-MPC8309 or for MPC8309?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any code example for TWR-MPC8309 or for MPC8309?

Jump to solution
3,443 Views
sergeygordienko
Contributor I

Hi. I'm trying to get started with MPC8309 programming and I'm looking for code examples or demos. any help would be appreciated. I'm interested in ethernet interface and HDLC controller.

Labels (1)
1 Solution
2,836 Views
yipingwang
NXP TechSupport
NXP TechSupport

In MPC8309 Linux BSP, there is a file ucc_tdm_framer.c in Kernel driver can be used as a reference, I have attached it, MPC8309 Linux BSP can be downloaded from MPC8309: Low-Power PowerQUICC II Pro Processor with DDR2, eSDHC, 128-ch. HDLC/TDM, 10/100 Ethernet, ....

In addition, NetComm Software provides UCC HDLC driver, I also attached it for you, please download NetComm 4.4 from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=NetComm_Software&fpsp=1&tab=Design_To... if needed.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,837 Views
yipingwang
NXP TechSupport
NXP TechSupport

In MPC8309 Linux BSP, there is a file ucc_tdm_framer.c in Kernel driver can be used as a reference, I have attached it, MPC8309 Linux BSP can be downloaded from MPC8309: Low-Power PowerQUICC II Pro Processor with DDR2, eSDHC, 128-ch. HDLC/TDM, 10/100 Ethernet, ....

In addition, NetComm Software provides UCC HDLC driver, I also attached it for you, please download NetComm 4.4 from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=NetComm_Software&fpsp=1&tab=Design_To... if needed.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,836 Views
sergeygordienko
Contributor I

Thank you for this files

0 Kudos
Reply