Is there any IBIS model for p2020?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any IBIS model for p2020?

1,203 Views
djw1987419
Contributor I

Is there any IBIS model for p2020? I couldn't find it on NXP website?

0 Kudos
Reply
1 Reply

1,123 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The P2020 IBIS model can be provided under non-disclosure agreement (NDA) only. To obtain additional information please create a Technical Case:

https://community.nxp.com/thread/381898

-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore
-------------------------------------------------------------------------------

0 Kudos
Reply