Is the software and micro code compatible when upgrading from MPC8560 to MPC8569

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the software and micro code compatible when upgrading from MPC8560 to MPC8569

1,234 Views
wchen
Contributor I

We are evaluating upgrading from MPC8560 to MPC8569. Will the the micro code be compatible between the two chips? We are supporting SS7 MTP2 and LAPD on it. Besides BSP (board support packet) changes, will the OS and application software need some change?

Thanks,

0 Kudos
Reply
1 Reply

1,166 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The micro code patches are not compatible between the two chips. However the MPC8569 QUICC engine has MCC which is slightly extended MCC of the MPC8560 CPM. It supports SS7. I recommend look into QUICC Engine Block Reference Manual with Protocol Interworking. See chapter 23.1.2 Comparison with MPC82xx CPM MCC.

You can download this manual using link on the MPC8659 nxp page

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...

Yes the BSP is bounded with particular Linux kernel. So you need use that kernel if you do not want to get additional problems. There is no general answer if application software need for some changes. Just try and test. Some application may require for changing.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply