Glueless interface of SDRAM with MPC8270

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Glueless interface of SDRAM with MPC8270

1,007 次查看
toltol
Contributor II

Hi i am using 12 SDRAMs with my MPC8270 and it says that it uses glues-less interface of SDRAM and other peripherals. 

Because of 12 SDRAM i am not able to do use my bus at 100Mhz because of signal integrity issues. As load is too high and 60x bus is not able to drive the SDRAM.

So can i use buffers in between SDRAM and PowerPC MPC8270?

I am confused because it says glue less interface, so is glue less interface must or optional?

pastedImage_1.png

标记 (2)
0 项奖励
回复
1 回复

845 次查看
alexander_yakov
NXP Employee
NXP Employee

Sorry for delayed response to this topic.

No, glue-less interface is not must. Moreover, external buffers are explicitly mentioned as supported - timing of all SDRAM control lines (except CS) may be changed accordingly. Please look MPC8280 Reference Manual, Table 11-8, the description of PSDMR[BUFCMD] field.

Note that CS line can not be buffered.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复