Enabling MPC8360 ENET3 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling MPC8360 ENET3 interface

1,700件の閲覧回数
kirankumartanka
Contributor I

We have designed a board based on MPC8360. In this board, we are using four Ethernets: ENET1, ENET2, ENET3 and ENET6. ENET1 and ENET2 are configured for GIG interface while ENET3 and ENET6 are used for 100Mbps (Fast Ethernet mode) using RMII interface. The PHY being used on the ENET3 interface is KSZ8031RNL from Micrel. The Gig interfaces are up using the dtb attached. How do we enable ENET3 and ENET6 in 100Mbps? I modified the dtb for ENET3 alone but it was not coming up!!!!

ラベル(1)
0 件の賞賛
返信
1 返信

1,575件の閲覧回数
Pavel
NXP Employee
NXP Employee

Try to see if it is software issue or hardware issue is to configure the loopback mode by setting GUMR[DIAG] = 01. If the lookback works, then issue is with hardware: pin configuration error, clock, PHY,  or signal problem; if the loopback fails, it is with software configuration problem.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信