Documents related to MPC8323E-RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Documents related to MPC8323E-RDB

1,655件の閲覧回数
narreddisivapra
Contributor II

Hi,

      I am using MPC8323E-RDB Board. I had downloaded iso image for that board. Can you send or suggest any documents regarding to building linux kernel for this board using LTIB in detail?

Thanks & Regards,

Siva Prakash.

0 件の賞賛
返信
3 返答(返信)

1,527件の閲覧回数
narreddisivapra
Contributor II

I am building Ltib from the iso image of MPC8323E-RDB, by mounting it at /mnt/cdrom, then I ran ./ltib. After this I checked /mnt/cdrom/ltib is present. After restarting the system(because of some reasons), the /mnt/cdrom/ having no files which are mounted when I run mount command. Are they temporary in nature.? Is it required to mount at every time when booting the PC.?

0 件の賞賛
返信

1,527件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, if you mount iso image by "mount" command, than this will work until reboot. If you want to mount this image permanently, than please do this through "fstab".

Please keep in mind that questions like "How to permanently mount iso image in your Linux workstation" are general Linux questions. If you are not familiar with these type questions, please welcome to:

The Linux Documentation Project  

0 件の賞賛
返信

1,527件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look the contents of /help/ folder of the downloaded *.iso image

0 件の賞賛
返信