Debugging DMA corruption - MPC8555 - Trace Buffers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging DMA corruption - MPC8555 - Trace Buffers

2,285件の閲覧回数
dijo
Contributor III

Hi Pavel,

we were able to locate the document and see the trace buffer  in action.

We were unable to find the right settings to trace a write over PCI/and through the Core to a DDR location (0x0eb00000) .

We tried using the following settings -

pastedImage_2.png

Do you see something which we overlooked, or did wrong?

Thanks in advance.

0 件の賞賛
返信
2 返答(返信)

2,048件の閲覧回数
LPP
NXP Employee
NXP Employee

It's good but i suggest to set "trace only in TRACE event" flag.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,048件の閲覧回数
dijo
Contributor III

Thanks again, Pavel!

Yes it works!

Would be great if you could tell how it works.What the "TRACE" implies?

0 件の賞賛
返信