DMA driver of MPC8308RDB BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA driver of MPC8308RDB BSP

1,501 Views
rettozero
Contributor I

Dear all,

I use MPC8308E in my design, and communicated it with FPGA througn local bus. And I want to use DMA to manage data movement between them. 

However, I can not find the responding DMA driver for mpc8308.(the old one, such as file" fsl_dma.c" is not suitable , i think). Can anyone tell me where to get the source code?

Thanks in advance. 

Tags (1)
0 Kudos
Reply
3 Replies

1,291 Views
alexander_yakov
NXP Employee
NXP Employee

MPC8308 processor has DMA engine similar to DMA engine used in MPC8349 processor. So, I think you can use MPC8349 driver fsldma.c with very little modifications.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,291 Views
rettozero
Contributor I

Thanks very much.

0 Kudos
Reply

1,291 Views
rettozero
Contributor I

I have forgot to say, I use the MPC8308RDB bsp, and search linux driver support for mpc8308 DMA

0 Kudos
Reply