DDR configuration and validation through QCVS tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR configuration and validation through QCVS tool

2,008 Views
Irfan3
Contributor III

Hi team,

I have one query. Is RCW required during DDR intialization and validation through QCVS tool?

 

Currently I have done hard-coded RCW and I am trying to use QCVS tool for DDR but it is throwing error as "DDR configuration incorrect. DINIT was not cleared by hardware" . 

Can anyone suggest what could be the issue??

Fyi, I am using custom t2081 board.

Thanks and regards

Irfan

0 Kudos
Reply
3 Replies

2,005 Views
ufedor
NXP Employee
NXP Employee

> Is RCW required during DDR intialization and validation through QCVS tool?

Valid RCW in the selected configuration source Flash is a must for normal operation of the QCVS DDR Tool.

0 Kudos
Reply

2,000 Views
Irfan3
Contributor III

Hi EUFEDOR,

 

Thanks for your quick response

So from your statement I can assume that DDR validation will not work with hard-coded RCW settings. It will work only with NOR/NAND based flash source only.

 

Because currently I have used hard-coded RCW settings for DDR validation through QCVS tool.

 

Thanks and regards

Irfan

0 Kudos
Reply

1,993 Views
ufedor
NXP Employee
NXP Employee

Your understanding is not correct.

Hard-coded RCW option cannot be used when DDR Tool is running.

0 Kudos
Reply