DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable

1,679 Views
kaurnakarhv
Contributor II

DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable:

Can this register value be enabled/disabled during run time?

Can anyone show insight on this?

Thanks.

Regards,

Karunakar

Labels (1)
2 Replies

1,367 Views
lunminliang
NXP Employee
NXP Employee

Hello Kaurnakar HV

Yes, you can change that. But it's not recommend to do this on-the-fly. Based on experience from our engineer, this could be problematic to guarantee the pipeline of DDR transactions will not cause a read to data with uninitialized ECC.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,367 Views
kaurnakarhv
Contributor II

Thanks for sharing the information.

Can you please elaborate more on this -

"This could be problematic to guarantee the pipeline of DDR transactions will not cause a read to data with uninitialized ECC"?

0 Kudos
Reply