DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable

1,765 次查看
kaurnakarhv
Contributor II

DDR_SDRAM_CFG[ECC_EN] ECC Enable/Disable:

Can this register value be enabled/disabled during run time?

Can anyone show insight on this?

Thanks.

Regards,

Karunakar

标签 (1)
2 回复数

1,453 次查看
lunminliang
NXP Employee
NXP Employee

Hello Kaurnakar HV

Yes, you can change that. But it's not recommend to do this on-the-fly. Based on experience from our engineer, this could be problematic to guarantee the pipeline of DDR transactions will not cause a read to data with uninitialized ECC.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,453 次查看
kaurnakarhv
Contributor II

Thanks for sharing the information.

Can you please elaborate more on this -

"This could be problematic to guarantee the pipeline of DDR transactions will not cause a read to data with uninitialized ECC"?

0 项奖励
回复