Compiling kernel 3.10 for mpc8309twr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling kernel 3.10 for mpc8309twr

1,712 Views
mdmuazzam
Contributor III

HI,

    I want to compile and load kernel 3.10 in mpc8309twr board ,whose BSP has only 2.6.33.7 kernel. So is is possible to upgrade kernel for above architecture.

Thanks

Muazzam(india)

0 Kudos
Reply
2 Replies

1,610 Views
Pavel
NXP Employee
NXP Employee

Look at information on the following page about kernel upgrade (http://www.berkes.ca/guides/linux_kernel.html).


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,610 Views
mdmuazzam
Contributor III

hi ,

it seems to be invalid link. not able to access it

thanks

0 Kudos
Reply