Compatibility between different MPC8309 core frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compatibility between different MPC8309 core frequency

1,019 次查看
brunoschmitt
Contributor I

I would like to know if part MPC8309CVMAGDCA (which runs at 400MHz) is 100% compatible with the MPC8309VMADDCA (which runs at 266MHz)? By compatible I mean if I just replace the 266MHz one by the 400MHz all functionalities will be the same, or it is needed to change any component around it (crystal and so on).

Thanks in advance!

标签 (3)
0 项奖励
回复
1 回复

876 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, they are 10% compatible. If you just replace 266 Mhz part by 400 Mhz part in 266 Mhz design, it will work at 266 Mhz without any changes required.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复