Code-Worrier programming corruption with NOR flash in T2080RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code-Worrier programming corruption with NOR flash in T2080RDB

跳至解决方案
2,794 次查看
singhawadhesh
Contributor I

Hi Team,

I was experimenting with NOR of T2080RDB and I have flashed U-boot with code-worrier in alternate bank of it. After making dump of that, I have compared it with actual file loaded into it with beyond compare (after converting both into HEX). I am finding there is mismatch in the dump data and the loaded file and unable to boot completely. When I am checking those locations (0xEBF4A19C) in memory window of debug, I am getting 0x4C00018C at every corrupted locations.

Please let me know the possible issue.

Thanks for your support.

Regards,

Awadhesh

0 项奖励
回复
1 解答
2,777 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please upgrade to CodeWarrior 10.5.2 to check whether this problem could be resolved.

Please open CodeWarrior IDE, please click Help->Install New Software->Available Software Sites, please select "CodeWarrior Power Architecture v10.5.2 Release, click drop down list at "Work with", then select "CodeWarrior Power Architecture v10.5.2 Release - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/COMPILER", then install CodeWarrior 10.5.2 step by step.

 

在原帖中查看解决方案

1 回复
2,778 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please upgrade to CodeWarrior 10.5.2 to check whether this problem could be resolved.

Please open CodeWarrior IDE, please click Help->Install New Software->Available Software Sites, please select "CodeWarrior Power Architecture v10.5.2 Release, click drop down list at "Work with", then select "CodeWarrior Power Architecture v10.5.2 Release - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/COMPILER", then install CodeWarrior 10.5.2 step by step.