Can not find file "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can not find file "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib"

1,513 次查看
maojiu
Contributor I

It can not find the files "u-boot-2010.06-mpc8306som-support-v2.patch.md5" and "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib". They are not in "www.bitshrine.org/gpp", though they are supposed to be there according to the output messages after running the command "./ltib". Where can I find the two files?

标记 (3)
0 项奖励
回复
2 回复数

1,341 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Which Linux BSP ISO did you install?

Actually in the u-boot spec u-boot-2010.06-mpc8306som.spec.in, there is no this patch u-boot-2010.06-mpc8306som-support-v2.patch listed.

Thanks,

Yiping

1,341 次查看
maojiu
Contributor I

Thank you for your reply. Finally I find the patch.

0 项奖励
回复