Can i use buffer on PCI bus of MPC8270?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i use buffer on PCI bus of MPC8270?

895件の閲覧回数
muhammadahmed47
Contributor II

I am interfacing MPC8270 with one FPGA and second FPGA on PMC Slot.

When PMC Card is inserted IBIS simulation works fine for PCI Bus.

Problem occurs when i remove the PMC card and now only FPGA is connected, and i causes reflections to come back and it destroys the signal.

Can i use the buffer in the PCI Path and if yes then how i can control the direction of that buffer. Thanks

0 件の賞賛
返信
1 返信

828件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

I do not see any buffer control signal in PCI signals. Please look MPC8280 Reference Manual, Chapter 6 for signal descriptions.

Here is a direct link to this document:

https://www.nxp.com/docs/en/reference-manual/MPC8280RM.pdf


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信