Can anyone explain MPC8306's uart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can anyone explain MPC8306's uart

1,114 Views
leimao
Contributor II

In one address 0x4500, It have 3 register. receiver buffer register. transmitter holding registers and Divisor least significant byte register. The 3 register in one address. How could I deal with that? I don't know what register I read or write

0 Kudos
Reply
2 Replies

996 Views
scottwood
NXP Employee
NXP Employee

That register is normally the transmitter holding register when you write to it, and the receiver buffer register when you read from it.  When you put the UART into a special mode it becomes the divisor least significant byte register.

Note that this UART is almost identical to a standard 16550 (e.g. as found on PCs), so any examples or tutorials you find for programming a standard UART would be applicable.

0 Kudos
Reply

996 Views
addiyi
NXP Employee
NXP Employee

Before reading from that address you should look at UIIR register. Please take a look in 8306 RM at chapter 18.3.1.5. Also, you can take a look in 8306SOM_serial project included in CW ( serial driver is already implemented in CodeWarrior as an example).

Adrian

0 Kudos
Reply