Can RCW be configured to boot from NOR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can RCW be configured to boot from NOR

跳至解决方案
1,929 次查看
muaxi8
Contributor V

Can the T4240 custom board be configured to boot from NOR Flash ? and if so, what is the address of

NorFlash programming RCW? I don't see that address in the document 《QorIQ-SDK-2.0-1703-IC

Rev0.pdf》

Documentation is given for programming RCW from I2C eeprom。

I used CodeWarrior to program RCW to the 0xe8000000 address, but the board wouldn't bring up

标记 (1)
0 项奖励
回复
1 解答
1,909 次查看
yipingwang
NXP TechSupport
NXP TechSupport

RCW is put at the begging of NOR flash.

In u-boot, RCW address is 0xE8000000.

In CodeWarrior initialization file C:\Freescale\CW_PA_v10.5.1\PA\PA_Support\Initialization_Files\QorIQ_T4\T4240QDS_init_sram.tcl, NOR flash is defined as the following.

# 0xE8000000 0xEFFFFFFF TLB1_4 NOR 128M

So in CodeWarrior, RCW address is also at 0xE8000000 .

You could reset the target board and dump NOR flash to check whether the read RCW image is correct.

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,910 次查看
yipingwang
NXP TechSupport
NXP TechSupport

RCW is put at the begging of NOR flash.

In u-boot, RCW address is 0xE8000000.

In CodeWarrior initialization file C:\Freescale\CW_PA_v10.5.1\PA\PA_Support\Initialization_Files\QorIQ_T4\T4240QDS_init_sram.tcl, NOR flash is defined as the following.

# 0xE8000000 0xEFFFFFFF TLB1_4 NOR 128M

So in CodeWarrior, RCW address is also at 0xE8000000 .

You could reset the target board and dump NOR flash to check whether the read RCW image is correct.

 

0 项奖励
回复