CCSProtocolPlugin : Error writing memory [CCS last error: Scan timeout ]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCSProtocolPlugin : Error writing memory [CCS last error: Scan timeout ]

3,302 次查看
padmakar
Contributor I

Hello NXP Experts,

Currently, I am working on the custom board which involves a Discrete DDR3L (MT41K512M16VRN-107 IT:P) interface with T2081. I have some questions regarding the DDR3L memory interface on T2081.

I have configured the .rcw, .tcl, .bin file as per the T2080RM.

1. I created the new project and then selected the "T2081QDS_init_sram -2.tcl" file for debugging the project. I have attached the .tcl file below.

2. I can debug successfully and flash on NOR devices as well.

3. Now I want to run DDR and initialize the DDR for that I have made changes in the "T2081QDS_init_core.tcl" file as per the T2080RM DDR memory map and datasheet of micron (MT41K512M16VRN-107 IT:P). I have attached the file below.

4. While I am debugging the ''T2081QDS_init_core.tcl'' file that time I am facing the error: CCSProtocolPlugin : Error writing memory [CCS last error: Scan timeout ]. I have attached the screenshot below.

5. In the QCVS tool, I have configured the registers as per the datasheet and T2080RM but I am also facing an error: D_INIT was not cleared by hardware. I have attached the screenshot below.

My Concern is, where I will use ''init_core.tcl'' and ''init_sram.tcl'' files and how I will configure the DDR registers in QCVS or init_core.tcl file.

 

Referred Documents:

1. T2080RM Rev. 4, 04/2021

2. QCVS_DDR_User_Guide Reference Manual 4.x, 02/2016

3. T2080RDBPCUG User Guide Rev. 1, 08/2021

4. MT41K512M16VRN-107 IT:P Datasheet.

 

CodeWarrior information:

CodeWarrior for Power Architecture
Version: 10.5.1
Build Id:160128

Find the attached documents.

Please give your valuable support/guidance.

 

Thanks and regards,

Padmakar

标签 (2)
0 项奖励
回复
1 回复

2,604 次查看
jayviva
Contributor I

 @padmakar Were you able to solve this issue?

0 项奖励
回复