Booting fail with CONFIG_PROFILE_ALL_BRANCHES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting fail with CONFIG_PROFILE_ALL_BRANCHES

1,866件の閲覧回数
arnobghosh
Contributor I

I am trying to booting profile all branches kernel in ep8248e board which has Freescale MPC8248 processor.

Kernel booting is failing when CONFIG_PROFILE_ALL_BRANCHES is enabled in MPC8241 processor.

It gets stuck after Finalizing device tree ....

Memory <- <0x0 0x8000000> (128MB)

zImage starting: loaded at 0x00900000 (sp: 0xf0001d20)
Allocating 0x8d2838 bytes for kernel ...
gunzipping (0x00000000 <- 0x0090e000:0x00ca6378)...done 0x880dc0 bytes

Linux/PowerPC load:
Finalizing device tree... flat tree at 0xcb3300

0 件の賞賛
返信
3 返答(返信)

1,476件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please specify which Linux BSP you are using, and where it was obtained from?


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,476件の閲覧回数
arnobghosh
Contributor I

Linux BSP is build from git://git.freescale.com/ppc/sdk/linux.git

Git tag checkout : fsl-sdk-v1.4

0 件の賞賛
返信

1,476件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

I do not see MPC8248 processor listed as supported in SDK 1.4

0 件の賞賛
返信