Boot secondary cpu from u-boot with the TWR-LS1021A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot secondary cpu from u-boot with the TWR-LS1021A

1,205件の閲覧回数
yasetoliva
Contributor I

Hello,

I've been trying without success to launch the secondary cpu from u-boot. I'm not sure about the procedure I'm implementing and I'd appreciate some help. Is there a link describing this procedure?

Best regards,

Yaset

0 件の賞賛
返信
1 返信

1,030件の閲覧回数
yasetoliva
Contributor I

Hello,

In case it can be helpful, the following procedure has worked for us:

1. Holdoff release (see function holdoff_release )

2. Set boot address (see function set_second_boot_addr )

3. Execute sev instruction (ex. asm("sev"))

Below the assembler code :

#define CONFIG_SYS_IMMR                             0x01000000
#define CONFIG_SYS_FSL_GUTS_ADDR        (CONFIG_SYS_IMMR + 0x00ee0000)
#define DCFG_CCSR_BRR                                0x0E4
#define DCFG_CCSR_SCRATCHRW1               0x200

.globl holdoff_release
holdoff_release:
    @ Clear and Get the correct CPU number
    movw    r1, #0xf01
    and r1, r1, #0xff

    @ Get DCFG base address
    movw    r4, #(CONFIG_SYS_FSL_GUTS_ADDR & 0xffff)
    movt    r4, #(CONFIG_SYS_FSL_GUTS_ADDR >> 16)

    @ Release on target CPU
    ldr r2, [r4, #DCFG_CCSR_BRR]
    mov r6, #1
    lsl r6, r6, r1  @ 32 bytes per CPU

    rev r6, r6
    orr r2, r2, r6
    str r2, [r4, #DCFG_CCSR_BRR]

.globl set_second_boot_addr
set_second_boot_addr:
    @ Get DCFG base address
    movw    r4, #(CONFIG_SYS_FSL_GUTS_ADDR & 0xffff)
    movt    r4, #(CONFIG_SYS_FSL_GUTS_ADDR >> 16)

    @ Set secondary boot address
    @ldr r6, r0
    mov r6, r0
    rev r6, r6
    str r6, [r4, #DCFG_CCSR_SCRATCHRW1]

    @ Return written
    mov r0, r6

0 件の賞賛
返信