About MPC8548E Power Sequencing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MPC8548E Power Sequencing

1,806 Views
youngho_cho
Contributor II

Hello, I'm Youngho.

I want to know power sequencing of MPC8548E.

According to its datasheet, MPC8548EEC, power sequencing is just 2 steps as follows:

   1. V_DD, AV_DD_n, BV_DD, LV_DD, OV_DD, SV_DD, TV_DD, XV_DD.

   2. GV_DD.

  And, the NOTE is as follows:

   Note1: Items on the same line have no ordering requirement with respect to one another. Items on separate lines must    be ordered sequentially such that voltage rails on a previous step must reach 90% of their value before the voltage    rails on the current step reach 10% of theirs.

   Note 2: In order to guarantee MCKE low during power-up, the above sequencing for GV_DD is required. If there is no    concern about any of the DDR signals being in an indeterminate state during power-up, then the sequencing for    GVDD is not required.

   Note 3: From a system standpoint, if any of the I/O Power supplies ramp prior to the V_DD core supply, the I/Os    associated with that I/O supply may drive a logic one or zero during power-up, and extra current may be drawn by the    device.

As I understood above, power sequencing is that the core powers is first powered up and then the I/O powers is next.

So, power sequencing I thought is as follows:

   1.V_DD

   2.AV_DD_n, SV_DD, XV_DD

   3.BV_DD, OV_DD, LV_DD, TV_DD

   4.GV_DD

Am I right?

0 Kudos
Reply
1 Reply

1,741 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

For sure V_DD to AV_DD_n delay is not required. Typically AV_DD_n is V_DD applied via PLL Power Supply Filter Circuit (see MPC8548E PowerQUICC III Family Bring-Up Guide). IO power should be delayed if any IO pin associated with it can harm system f.i. due to contention. I think the serdes io pins are quite harmless. In any case your power sequence is correct too if all supplies reach their stable values within 50 ms.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply