the fs1b pin of FS6500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the fs1b pin of FS6500

1,092 Views
JhonYF
Contributor III

JhonYF_0-1716267644729.png

After reset, the driver program will attempt to clear error counts and release the FS1B pin, so the situation depicted in the diagram will not occur.What was the problem?

 

0 Kudos
Reply
1 Reply

1,086 Views
guoweisun
NXP TechSupport
NXP TechSupport

做到哪一步了?RSTB release了?然后就是写一次WD 退出INIT阶段在256ms以内如果写错了或者超过了256ms才去写RSTB也会reset一下再次给机会去写WD进入下一个阶段,然后再继续feed WD 去减少FAULT ERROR COUNTER 值,如果期间的每一次feed WD错误都会导致fault errorcounter的增加这样就不会release FS1B/FS0B

0 Kudos
Reply