mc33664+33771c TPL communication debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc33664+33771c TPL communication debug

Jump to solution
2,040 Views
leonggz
Contributor II

in a customized board we are using tpl between 33664 and 33771c and i'm getting comm timeout on all statuses. by closer look, i can see the RX clocks are present but not 50% duty square wave but more like 10-20% pulses... i wonder if anyone can shed some light on what might be the possible causes in the hw(?)

0 Kudos
Reply
1 Solution
1,928 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Guoliang,

please download and check the AN12626 from the MC33771C product page and please refer to the section 13.2.6 in the MC33771C datasheet. To check if you have used the recommended components for the TPL communication interface. Please share your schematic with voltage levels and part values.

Please consider purchasing the some of our evaluation boards with MC33771C+MC33664+BATT14CEMULATOR. For example MPC5775B-BATTERYSYSTEM kit. Or FRDMDUAL33664EVB, RD33771CDSTEVB and BATT-14CEMULATOR. Then you can use your own MCU to communicate with the FRDMDUAL33664EVB through the SPI interface.

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
1,929 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Guoliang,

please download and check the AN12626 from the MC33771C product page and please refer to the section 13.2.6 in the MC33771C datasheet. To check if you have used the recommended components for the TPL communication interface. Please share your schematic with voltage levels and part values.

Please consider purchasing the some of our evaluation boards with MC33771C+MC33664+BATT14CEMULATOR. For example MPC5775B-BATTERYSYSTEM kit. Or FRDMDUAL33664EVB, RD33771CDSTEVB and BATT-14CEMULATOR. Then you can use your own MCU to communicate with the FRDMDUAL33664EVB through the SPI interface.

With Best Regards,

Jozef

0 Kudos
Reply