I found that if I'm in Debug Mode and haven't executed EXIT_DBG_MODE, FS0B_SNS and FS1B_SNS will be 0 / SENSED LOW. In this case, if I connect TP88 to 5V, I can get a SHORT TO HIGH DETECTED to set FS0B_DIAG = 1, and if I connect TP11 to 5V, I can get a SHORT TO HIGH DETECTED to set FS1B_DIAG = 1. However, if I'm in NORMAL Mode and have released FS0B and FS1B, because FS0B_SNS and FS1B_SNS will be 1 / SENSED HIGH, I cannot perform a check on FS0B_DIAG and FS1B_DIAG. This is because FS0B_DIAG and FS1B_DIAG are initially 1 / SHORT TO HIGH DETECTED, even though I haven't Input 5V to TP88 and TP11.


When FS_STATES = 10 / Safety Outputs not released, connecting TP88 to 5V triggers a short to high detected and gives FS0B_DIAG = 1. Connecting TP11 to 5V triggers a short to high detected and gives FS1B_DIAG = 1.

When FS_STATES = 11 / Normal, I connected TP88 / TP11 to 5V, but FS0B_DIAG / FS1B_DIAG is always 0 / NO FAILURE.

This means that FS0B_DIAG / FS1B_DIAG detection is not possible when FS_STATES = 11.