VR5510 Standby mode exit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VR5510 Standby mode exit

跳至解决方案
4,645 次查看
brian_w
Contributor III

Hi all,

       Recently,i am trying to make the VR5510 and S32G exit the Standby mode. After entering the standby mode successfully, I pull up the PMIC_STBY_MODE_B to let the PMIC exit standby mode. Then the PMIC will pull down PGOOD, and this will reset the whole S32G.

   Is this phenomenon correct? If the PMIC pull down the PGOOD after existing from standby mode, how can S32G use fast boot when exit standby mode?

0 项奖励
回复
1 解答
4,584 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hardware configurations must be done before entering Standby mode.

PGOOD and RSTB pins should be externally pulled up to VPRE.

VPRE remains on during the Standby mode, and so, PGOOD and RSTB remain HIGH during the Standby mode.

These states of the pins prevent the S32G to reset when the VR5510 enters Standby mode.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,589 次查看
brian_w
Contributor III

From the G2 datasheet, when existing from standby, POR_B and RESET_B should remain high. How can we achieve this? Are there some configurations in VR5510 to achieve this?

brian_w_0-1698201932788.png

 

 

0 项奖励
回复
4,585 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hardware configurations must be done before entering Standby mode.

PGOOD and RSTB pins should be externally pulled up to VPRE.

VPRE remains on during the Standby mode, and so, PGOOD and RSTB remain HIGH during the Standby mode.

These states of the pins prevent the S32G to reset when the VR5510 enters Standby mode.

0 项奖励
回复
4,624 次查看
guoweisun
NXP TechSupport
NXP TechSupport

What do you mean for PMIC_STBY_MODE_B? does PMIC_STBY_MODE_B same with VR5510 STBY pin?

0 项奖励
回复
4,610 次查看
brian_w
Contributor III

Yes, it's the same as STBY pin of VR5510

brian_w_0-1698131801486.png

 

0 项奖励
回复
4,629 次查看
KalaimaniArumugamdev
Contributor III

Hi @brian_w 

       There is chance the Reset and PGOOD  are sharing  in the same  pin. Because of this block diagram,

 

Screenshot 2023-10-23 09.28.30.png

0 项奖励
回复
4,606 次查看
brian_w
Contributor III

Hi,

When the PMIC exist from standby, the RESET_B must will be pulled low, and the RESET_B is shareing with POR_B, so the POR_B will be pulled low too. Is this what you mean?

From the G2 datasheet, when existing from standby, POR_B and RESET_B should remain high. How can we achieve this?

brian_w_0-1698132029113.png

 

0 项奖励
回复