VR5510 Standby mode entry

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 Standby mode entry

ソリューションへジャンプ
3,821件の閲覧回数
leo_liu2
Contributor III

Hi all,

       Recently,i am trying to make the VR5510 and S32G enter the Standby mode.According to the AN12952 and AN12880,the following two steps were performed:

(1)I send a enter standby mode command to the VR5510 through IIC by calling the Pmic_Ipw_SetMode() function firstly.

(2)And then,i pull down the PMIC_STBY_MODE_B pin by calling the Power_Ip_SetMode().

    After finishing the step mention above,i found that the SOC do not enter standby mode but reset repetitive.Is there any wrong i have do or any step i have miss?The purpose i want is to let the SOC(S32G-VNP-RDB2)  and VR5510 enter standby mode.

タグ(2)
0 件の賞賛
返信
1 解決策
3,798件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Huawei,

please refer to the section 5.4.1.2 in the AM12880. I see you want to use the Safe transition mode, the I2C bus command and the STBY pin. For this case, please make sure, that you have set the bits 4 and 5 in the CFG_2_OTP register. The STBY_SAFE_DIS_OTP bit must be set to logic 0 and the STBY_WINDOW_EN_OTP must be enabled.

JozefKozon_0-1665728922235.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,799件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Huawei,

please refer to the section 5.4.1.2 in the AM12880. I see you want to use the Safe transition mode, the I2C bus command and the STBY pin. For this case, please make sure, that you have set the bits 4 and 5 in the CFG_2_OTP register. The STBY_SAFE_DIS_OTP bit must be set to logic 0 and the STBY_WINDOW_EN_OTP must be enabled.

JozefKozon_0-1665728922235.png

With Best Regards,

Jozef

0 件の賞賛
返信
3,707件の閲覧回数
leo_liu2
Contributor III

Hi Jozef,

     My problam has been solved,thanks for your reply!

0 件の賞賛
返信
2,439件の閲覧回数
Yang_C
Contributor IV

Hi Leo,

May I ask how you resolved your problem? I am haing the same issue recently.

Looking forward to your reply. 

Thanks

タグ(1)
0 件の賞賛
返信
3,702件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Huawei,

you are very welcome. I am glad, that your issue is solved.

With Best Regards,

Jozef

0 件の賞賛
返信