UJA1169 sleep current issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UJA1169 sleep current issue

ソリューションへジャンプ
3,130件の閲覧回数
949147417
Contributor I

Hello,

    I have an issue with UJA1169 sleep current issue, when SBC in Sleep mode(V1&V2 are both off)sleep current is about 400uA, it is bigger than 65uA which defined in datasheet. By the way, customer has CAN partial networking requirement.

Capture.PNG

Why SBC has so high sleep current?

BR

0 件の賞賛
返信
1 解決策
3,012件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

You can try to test this current under CAN partial networking disable by setting PNCOK/CPNC bit as '0' in CAN control register.

Thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,013件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

You can try to test this current under CAN partial networking disable by setting PNCOK/CPNC bit as '0' in CAN control register.

Thanks!

0 件の賞賛
返信
3,012件の閲覧回数
949147417
Contributor I

ok,we solve it by stop CANoe,thanks

-Original-

0 件の賞賛
返信