UJA1169 sleep current issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1169 sleep current issue

Jump to solution
3,157 Views
949147417
Contributor I

Hello,

    I have an issue with UJA1169 sleep current issue, when SBC in Sleep mode(V1&V2 are both off)sleep current is about 400uA, it is bigger than 65uA which defined in datasheet. By the way, customer has CAN partial networking requirement.

Capture.PNG

Why SBC has so high sleep current?

BR

0 Kudos
Reply
1 Solution
3,039 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

You can try to test this current under CAN partial networking disable by setting PNCOK/CPNC bit as '0' in CAN control register.

Thanks!

View solution in original post

0 Kudos
Reply
2 Replies
3,040 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

You can try to test this current under CAN partial networking disable by setting PNCOK/CPNC bit as '0' in CAN control register.

Thanks!

0 Kudos
Reply
3,039 Views
949147417
Contributor I

ok,we solve it by stop CANoe,thanks

-Original-

0 Kudos
Reply