Hello Team,
I am using TJA1128 in my control board, which is the primary source 5V for Micro.
There is a failure with TJA, here are the info, could you let me know what could be the problem?
Note: LIN wake up is activated remote, I need to know why there is no 5V at VCC, and Reset is held LOW (may be under voltage at VCC)
| PIN | Measured Output in V |
| Wake1 | 7.93 |
| Wake2 | 7.93 |
| BAT | 13.36 |
| LIN | 12.68 |
| GND | |
| VCC | 0 |
| TXD/SDI | 0 |
| LIN_EN | 0 |
| RST | 0 |
| RXD | 0 |
| WWD | 0 |
Any ideas?
Any ideas on this?
Please share with the schematic!
Seems the SBC triggers the OVERTEMP mode.
which data you added?
Factor to consider,
TJA in my control board were working continuously for 78hrs at ambient temp of 65 deg, it failed at this point of time.
Interesting part is 4 samples failed between 70-90 hrs of continuous running at the same environment with the same issues.
So do you mean after power on SBC no VCC output? or after your high temperature test lost the VCC?
do you try to change new SBC test again?
Can you reproduce this issue with new SBC in your board?
If so please read datasheet page18 -----6.3.4.2 Restoring factory preset values