TJA1128 NO VCC output issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA1128 NO VCC output issues

5,653 次查看
Kavin_Kumaravel
Contributor II

Hello Team,

I am using TJA1128 in my control board, which is the primary source 5V for Micro. 

There is a failure with TJA, here are the info, could you let me know what could be the problem?

Note: LIN wake up is activated remote, I need to know why there is no 5V at VCC, and Reset is held LOW (may be under voltage at VCC)

PINMeasured Output in V
Wake17.93
Wake27.93
BAT13.36
LIN12.68
GND 
VCC0
  
TXD/SDI0
LIN_EN0
RST0
RXD0
WWD0
0 项奖励
回复
15 回复数

5,519 次查看
Kavin_Kumaravel
Contributor II

Any ideas?

0 项奖励
回复

5,520 次查看
Kavin_Kumaravel
Contributor II

Any ideas on this? 

0 项奖励
回复

5,645 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please share with the schematic!

0 项奖励
回复

5,638 次查看
Kavin_Kumaravel
Contributor II

Schematics

0 项奖励
回复

5,628 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Seems the SBC  triggers the OVERTEMP mode.

 

 

0 项奖励
回复

5,622 次查看
Kavin_Kumaravel
Contributor II
Currently, these data I have added is tested at 25 deg cel.
0 项奖励
回复

5,618 次查看
Kavin_Kumaravel
Contributor II
Measured voltage added to the initial question
0 项奖励
回复

5,620 次查看
guoweisun
NXP TechSupport
NXP TechSupport

which data you added?

 

0 项奖励
回复

5,643 次查看
Kavin_Kumaravel
Contributor II

Factor to consider,

TJA in my control board were working continuously for 78hrs at ambient temp of 65 deg, it failed at this point of time.

Interesting part is 4 samples failed between 70-90 hrs of continuous running at the same environment with the same issues.

0 项奖励
回复

5,616 次查看
guoweisun
NXP TechSupport
NXP TechSupport

So do you mean after power on SBC no VCC output? or after your high temperature test lost the VCC?

do you try to change new SBC test again?

 

0 项奖励
回复

5,612 次查看
Kavin_Kumaravel
Contributor II
When tested at high temp, over temp could trigger TJA to reset. Now I am testing at room temperature, But TJA is not recovered. Can you explain why is that case? Is this problem with register, incase of how do i do factory reset?
0 项奖励
回复

5,610 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Can you reproduce this issue with new SBC in your board?

 

0 项奖励
回复

5,606 次查看
Kavin_Kumaravel
Contributor II
No, at least not any time soon. Is it possible to do factory reset?
0 项奖励
回复

5,605 次查看
guoweisun
NXP TechSupport
NXP TechSupport

If so please read datasheet page18 -----6.3.4.2 Restoring factory preset values

0 项奖励
回复

5,603 次查看
Kavin_Kumaravel
Contributor II
I checked
All conditions passed, Vbat > Vth, LIN is held dominant and RSTN is low(0V) for more than 1 sec, but problem is RSTN is always LOW. I am assuming it means that SBC is not coming out of RESET loop?Any ideas why is that
0 项奖励
回复